Technical FAQs

Ask a Question

What type of hub can be used on a MA1000DS Circuit Breaker Enclosure?

Use watertight H (zinc) type or H-CP (chrome plated zinc) type. H and H-CP type of hubs are available for 1/2`` through 4`` conduit trade sizes.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.


CTA-ID : 2009648
Was this helpful?
What can we do to improve the information ?