Technical FAQs

Ask a Question

Can a GFM be wired without a neutral?

It may be used on a 3 wire system (without a neutral). It also may be used on a 4 wire system with a neutral, using the neutral CT. The system must be grounded in either case.

CTA-ID : 2010334
Was this helpful?
What can we do to improve the information ?