Technical FAQs

Ask a Question

What is the wire range on a PK**GTA ground bar<br />

The wire range is one # 14 to # 4 or two # 14 or #12 Copper. Also the wire range is one # 12 to # 4 or two # 12 or #10 Aluminum


CTA-ID : 2010324
Was this helpful?
What can we do to improve the information ?