Technical FAQs

Ask a Question

How can you tell the number of pins required for a 8501KP13V20 relay?

The number of pins (11) is determined by the control circuit and contact arrangement of the relay. The easiest way to determine the number of pins is to look at the wiring schematic or the socket selection data in the digest 171, 172 or 170.


CTA-ID : 2010094
Was this helpful?
What can we do to improve the information ?