Technical FAQs

Ask a Question

What is the part number for the computer cable that will allow connection to a Soft Starter using SoMove or the obsolete PowerSuite software?

Issue:
Customer wants to connect his ATS48 or ATS22 softstart to a PC using Schneider Electric's configuration software.

Product Line:
ATS48
ATS22

Environment:
All part numbers, all models

Cause:
Cable is required for the connection.

Resolution:
TCSMCNAM3N002P is a USB to RJ45 cable that includes the RS485 converter required to commmunicate to the softstart (and our current VFD products).

NOTE: The old cable kit part number VW3A8106 will also work but requires a DB9 serial port on the PC (or a USB to DB9 adapter)

The SoMove software is available for download from our website:  http://www.schneider-electric.us/en/product-range/2714-somove/?parent-subcategory-id=54405
Also required is the DTM Library for the product.

NOTE:  Powersuite has been obsolete for many years.  It is no longer supported and is not recieving updates.

 
Was this helpful?
What can we do to improve the information ?