Technical FAQs

Ask a Question

What do I have to add to the ATV28 to make it NEMA Type 1

Issue:   What do I have to add to the ATV28 to make it NEMA Type 1
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:  
By using the grey adhesive cover supplied with the drive from the factory and adding the Conduit Enterance Kit you will achieve a Type 1 rating.


 
Was this helpful?
What can we do to improve the information ?