Technical FAQs

Ask a Question

What is the part# for the 5` SS rod only for a 9049DRA32

Use 2- 9049T2S. These are extension pieces for the kit. There are fittings and components in the kit that are not sold separately. Therefore, be cautious if someone tries to purchase parts in lieu of the entire device.


CTA-ID : 2009853
Was this helpful?
What can we do to improve the information ?