Technical FAQs

Ask a Question

What type of hub can be used on a IK250DS Circuit Breaker Enclosure?

Use watertight H (zinc) type or H-CP (chrome plated zinc) type. H and H-CP type of hubs are available for 1/2`` through 4`` conduit trade sizes.


CTA-ID : 2009641
Was this helpful?
What can we do to improve the information ?