Technical FAQs

Ask a Question

Which type of fuse(s) do the 9422 flange mounted, variable depth fused disconnect switches accept?

They will accept the Class H and K fuse as standard. It will accept the Class R with a rejection clip. It will accept the Class J by moving the load side fuse base assembly to a pre-determined space closer to the switch.

CTA-ID : 2009630
Was this helpful?
What can we do to improve the information ?