Technical FAQs

Ask a Question

How do I size an enclosure for a drive?

Follow the information contained in the Installation Manual for enclosing drive in enclosure. The manual shows the total dissipated power in Watts as well as minimum clearance, minimum airflow, and stirring fan recommendations.
Contact the enclosure manufacturer for sizing the enclosure based on the thermal load (Watts loss) of the drive and minimum spacing requirements.


CTA-ID : 2010309
Was this helpful?
What can we do to improve the information ?