Technical FAQs

Ask a Question

A 9007MS01S0400 Has a hole on either side of the plunger on the horizontal plane. These are different from the holes on the veritcal plane above the nameplate. The holes do not go through to the bottom of the switch and are not threaded. Are these mounting holes? Can they be tapped?

The holes are shown on the drawing but the dimesions are not supplied. They were not intended for mounting the switch and we would not recommend tapping the holes for mounting purposes. The holes are used by manufacturing to secure the switch during production.


CTA-ID : 2010306
Was this helpful?
What can we do to improve the information ?