Technical FAQs

Ask a Question

What is the part number for the keypad remote mount kit for the ATS46?

Issue: What is the part number for the keypad remote mount kit for the ATS46?
 
Product Line: ATS46
 
Environment: All
 
Cause:  N/A
 
Resolution: VW3G46103

The kit includes the hardware, a 3 meter cable, connection modules, bezel and plastic cover suitable for mounting in a Type 12 enclosure.

This is the keypad remote mounting kit.

It does not include the VW3G46101U keypad. The keypad comes as part of the ATS46 and can be used with this kit.


 
Was this helpful?
What can we do to improve the information ?