Technical FAQs

Ask a Question

Is the SD9342 (fusible SD plug-in unit) obsolete?

Yes. However the SD75460 (circuit breaker plug-in unit) can be used to replace the obsolete SD9342.


CTA-ID : 2009623
Was this helpful?
What can we do to improve the information ?