Technical FAQs

Ask a Question

What are the mounting clearances required for the NEMA 3R EconoFlex unit.

The mounting clearances are Minimum 2`` from the outside of side hood on each side, 6`` on top & 12`` on bottom (Page 27 of the 30072-450-10 manual)

Additionally the unit MUST be mounted Vertically against a solid flat surface (Page 32 of the 30072-450-10 manual)

CTA-ID : 2010055
Was this helpful?
What can we do to improve the information ?