Technical FAQs

Ask a Question

What are the mounting clearances required for the NEMA 1 and NEMA 12 EconoFlex unit?

The mounting clearances are Minimum 3`` on each side, 6`` on top & bottom (Page 25 & 26 of the 30072-450-10 manual).

Additionally the unit MUST be mounted Vertically against a solid flat surface (Page 32 of the 30072-450-10 manual)


CTA-ID : 2010054
Was this helpful?
What can we do to improve the information ?