Technical FAQs

Ask a Question

Can the speed of the acceleration ramp be controlled by a voltage or current analog input on the ATS48?

No.

Soft starters are not designed to control the speed of the output by adjusting an analog input which is a function of a drive. Starters are voltage ramp designed and do not vary the frequency.


CTA-ID : 2009832
Was this helpful?
What can we do to improve the information ?