Technical FAQs

Ask a Question

Is the QMB310EX a complete kit for all 3 phase connections?

Issue:
Product features

Product Line:
QMB Branch Switches

Cause:
Installation

Resolution:
Yes one kit is required for each series D2 QMB, either twin or single units


CTA-ID : 2009614
Was this helpful?
What can we do to improve the information ?