Technical FAQs

Ask a Question

Can the GC-200 ground fault relay be adjusted while the equipment it protects is energized?

Yes, however if the device is adjusted to a value which cause the relay to go into pickup, the device will trip. Proper electrical safety procedures must be taken.


CTA-ID : 2009609
Was this helpful?
What can we do to improve the information ?