Technical FAQs

Ask a Question

How can you increase the frequency the ATV16 unit to run above 60hz because HSP will not go any higher?

Issue: How can you increase the frequency the ATV16 unit to run above 60hz because HSP will not go any higher?
 
Product Line: ATV16
 
Environment: All
 
Cause: HSP above 60Hz
 
Resolution: Before you can change the HSP setting you need to first verify that you are in the programming mode which means that switch 2 on keypad is in the on position.

Once confirm in programming mode in order to adjust high speed (HSP) you need to first go to the tFR maximum frequency parameter and adjust this up to the upper level limit desire speed to go to.  Then after adjusting this up can adjust HSP up to this value.


 
Was this helpful?
What can we do to improve the information ?