Technical FAQs

Ask a Question

Can the Altivar 58 drive be controlled by the keypad?

Yes.  The keypad has start and stop keys for keypad command.
Go to menu 4 (CtL). Set parameter LCC (Keypad Com) to YES.
To change the speed use the LFr parameter from the SEt or SUP menus.
LFr can be set as the default display in the SUP menu by displaying LFr and pressing ENT 2 times.


CTA-ID : 6828
Was this helpful?
What can we do to improve the information ?