Technical FAQs

Ask a Question

What is the electrical interlock for use with the HU365DS Series E2 Heavy Duty Safety Switch?

Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Environment;
Accessories

Cause:
Application

Resolution:

The HU365DS Series E2 used the EIK40601 for 1-NO/1-NC contacts or EIK40602 for 2-NO/2-NC contacts.


CTA-ID : 2010039
Was this helpful?
What can we do to improve the information ?