Technical FAQs

Ask a Question

Does the ATV66 unit have the capability to program a custom fault that will be indicated when triggered by external source.

Yes.

If the drive has the I/O extension module VW3A66201T / VW3A66202T installed a logic input can be programmed for customer fault in menu 7.4.

This customer fault is activated by a logic input and the active state can be programmed to be high or low.  The fault stopping method also is programmable.


CTA-ID : 2010036
Was this helpful?
What can we do to improve the information ?