Technical FAQs

Ask a Question

Does the ATV66 unit still stop when the customer fault is assigned and triggered off the terminal strip even though operating in serial communication mode?

No.

The unit can not be operated in terminal strip and serial communication mode both at the same time. If the unit is in serial communication mode then the customer fault input while triggered will not stop the drive. The only terminals active in serial mode is the ones assigned to forced local or stop / run permissive .


CTA-ID : 2010035
Was this helpful?
What can we do to improve the information ?