Technical FAQs

Ask a Question

Will the ATV28 HU29M2U run on single phase input for a three phase motor?

Yes it is designed to run a 230vac 3 phase motor from a 230 vac Single Phase input.

Also, all the following units are rated for single phase input and 3 phase output:
 HU09M2U , HU18M2U , HU29M2U , HU41M2U

CTA-ID : 2010034
Was this helpful?
What can we do to improve the information ?