Technical FAQs

Ask a Question

Can two 100A 2P (QE-VH) breaker be used in place of one 200A 2P (QE-VH) breaker in the EZML113200?

This is a misapplication of the device. Each tenant space is protected by one tenant circuit breaker only.

CTA-ID : 2009597
Was this helpful?
What can we do to improve the information ?