Technical FAQs

Ask a Question

Can the Altivar Drives be used as both a Master and Slave with the Modbus protocol?

All drives in the Altivar family are designed network slave devices only.
They can not be used as Masters in the network.


CTA-ID : 2010267
Was this helpful?
What can we do to improve the information ?