Technical FAQs

Ask a Question

Can a 9012 pressure switch be made to operate on rising pressure?

Yes, The 9012`s have SPDT or DPDT contacts. Wire the NO contact so that it will close when the pressure hits the high pressure set point.

CTA-ID : 2010027
Was this helpful?
What can we do to improve the information ?