Technical FAQs

Ask a Question

For a NEMA size 00 - 4 and 6 starter, what is the part number for the little plastic, normally closed contact on the overload?

It is 9998SO1.


CTA-ID : 2010024
Was this helpful?
What can we do to improve the information ?