Technical FAQs

Ask a Question

Does Square D offer a QO, 100 amp, 2-pole, 240V ac branch breaker that is Switch Duty rated?

Issue:
Product design

Product Line:
Miniature circuit breakers, load centers

Environment:
QO branch circuit breakers

Cause:
Application

Resolution:
The Switch Duty Rating (SWD) ONLY applies to 15 and 20amp breakers.  So Square D does NOT offer a 100amp, QO breaker with SWD rating.
Was this helpful?
What can we do to improve the information ?