Technical FAQs

Ask a Question

What is the optional lug that will accept (2) 2/0-350 kcmil wire per phase on a NSJ400 breaker

A 32510 lug for one side can be ordered that will be able to accept (2) 2/0-350MCM Cu and (2) 2/0-500MCM Al


CTA-ID : 2009805
Was this helpful?
What can we do to improve the information ?