Technical FAQs

Ask a Question

Customer has a PQ4210 that is horizontally mounting and also has a replacement in stock but it is for vertical mounting. What can he do as he does not have enough room for the vertical mounting?

PQ4210G is made to mount on busway that is running horizontally and also vertically. For a smaller profile, consider a circuit breaker plug-in unit - PFA32100GN. This only hangs below the busway 1.12 inches.

CTA-ID : 2009624
Was this helpful?
What can we do to improve the information ?