Technical FAQs

Ask a Question

What is the ATV28 RS485 Cable Pin Out for the newer units?

Issue:   What is the ATV28 RS485 Cable Pin Out for the newer units?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   Cable pinout
 
Resolution:   Terminal #5 is still D(A) on the new connection, 0V is still 2, 10V is still 7 but D(B) is now terminal 4 instead of the old terminal 3.

The old units have date code before 09/2001

Pin 1 on the RS485 port of drive is all the way to left and Pin 8 is right most Pin.


 
Was this helpful?
What can we do to improve the information ?