Technical FAQs

Ask a Question

Why is the W (width) dimension and the W/H (width w/handle) dimension the same on some safety switches?

In these cases, the handle would be flange mounted, not side mounted. The handle does not add any additional width to the device.

CTA-ID : 2009582
Was this helpful?
What can we do to improve the information ?