Technical FAQs

Ask a Question

Does the AO on the ATS48 require an external 24v power source to be used?

No.

The source is internal and if connect to AO and com get ma source corresponding to how have output configured.


CTA-ID : 2010247
Was this helpful?
What can we do to improve the information ?