Technical FAQs

Ask a Question

Can single pole QO breakers be installed in the CU12L400N, CU12L400B or CU12L400L devices?

Only QO 2 pole breakers can be used. The panel labeling states this fact. The use of single pole breakers would create issues concerning the 6 disconnect rule for service entrance devices.


CTA-ID : 2010241
Was this helpful?
What can we do to improve the information ?