Technical FAQs

Ask a Question

What is the operational ambient temperature range on the Altivar ATV66?

0-40 degrees C ( +32* to +104*F )


CTA-ID : 6992
Was this helpful?
What can we do to improve the information ?