Technical FAQs

Ask a Question

What Equipment Ground Kit is used with the DTU463AWK, Series F05 or F06, Double Throw Safety Switch?

The Equipment Ground Kit is factory installed in this device. Three lugs are provided, each accepting (1) #12 - 1/0 AWG aluminum or (1) #14 - 1/0 copper ground conductor.


CTA-ID : 2009569
Was this helpful?
What can we do to improve the information ?