Technical FAQs

Ask a Question

What Equipment Ground Kit is used with the DT363RB, Series F05, Double Throw Safety Switch?

The Equipment Ground Kit is factory installed in this device. Three lugs are provided, each accepting (1) #12 - 1/0 AWG aluminum or (1) #14 - 1/0 copper ground conductor.

CTA-ID : 2009560
Was this helpful?
What can we do to improve the information ?