Technical FAQs

Ask a Question

Why does the 8839 Flex58 when try to connect with power suite 1.4 get unsuccessful attempt each time try?

Confirm that using the correct com port, have the appropriate cabling for the unit trying to connect to and if this does not correct issue verify the com port baud rate is 19200 to match keypad port.

CTA-ID : 2009559
Was this helpful?
What can we do to improve the information ?