Technical FAQs

Ask a Question

Why does the analog output when set up for motor current in menu 2.2 indicate 19% when the unit is not even being told to run?

The display shows 19% or 20% because the analog output is set up for 4 to 20ma instead of 0 to 20ma.  
When set up for minimum 4ma then at 0 current still have 20% of 20ma as minimum output which is what the display corresponds to in menu 2.2.


CTA-ID : 2010237
Was this helpful?
What can we do to improve the information ?