Technical FAQs

Ask a Question

How can run status output be derived from an Altivar 58 drive?

The R2 relay can be programmed for run status. The R2A and R2C contacts will close when there is a valid run command.
Unlock the keypad. Remove all active logic input signals. Go to menu 5 (I-O menu).
Set r2 to run (Drive Running)

Or, the R2 relay can be programmed for Frequency Threshold Attained. The contacts will close when output frequency is at or greater than the frequency threshold.
Unlock the keypad. Remove all active logic input signals. Go to menu 5 (I-O menu).
Set r2 to FtA (Frequency Threshold Attained)
Go to menu 2 (SEt adjustments)
Set Ftd to a very low frequency such as 0.1.


CTA-ID : 2009905
Was this helpful?
What can we do to improve the information ?