Technical FAQs

Ask a Question

What is the number for the ``90 degree Angle Sealing Plate`` for LJB wireway?

It is referenced in the current Class 5100 catalog as a ``90 degree Connector``. Use:
LJB290C for the 2.5`` X 2.5``
LJB490C for the 4`` X 4``
LJB690C for the 6`` X 6``
LJB890C for the 8`` X 8``
LBJ12690C for the 12`` X 6``


CTA-ID : 2009989
Was this helpful?
What can we do to improve the information ?