Technical FAQs

Ask a Question

How do yo go back to factory default settings on an ATV66?

Unlock the keypad using the switch on the back of keypad (switch on left side toward the bottom facing back of keypad should be in the down position which is unlocked), go to menu number 10 in main menu which is called ACCESS LOCK and enter here to select either PARTIAL UNLOCK or TOTAL UNLOCK.  Then go to menu number 9 DRIVE INIT. and then select TOTAL FACATORY SETT. (or either partial fact. setting)

CTA-ID : 2009883
Was this helpful?
What can we do to improve the information ?