Technical FAQs

Ask a Question

Why cant an LA1SK20 adder deck be used on an CA3SK11 DC relay?

The coil is not strong enough to operate both sets of contacts effectively. They adder deck is configured so that it will only fit the CA2 AC relay.

CTA-ID : 2009775
Was this helpful?
What can we do to improve the information ?