Technical FAQs

Ask a Question

Does the ``O`` ring gasket come with the GS1AH110 operator for a NEMA 4/4X enclosure?

No because the GS1AH110 operator is for Type 1 and 12 indoor applications. You must use the GS1AH410 operator to get the O ring for Type 4/4X applications.

CTA-ID : 2009765
Was this helpful?
What can we do to improve the information ?