Technical FAQs

Ask a Question

Why does the ATV58HC19N4XZU come up with an INI from the keypad or when using Power Suite?

ATV58HC19N4XZU Drives with software versions V5.2IE09 or V5.3IE11 do not power up properly with V5.xIExx Keypads. They display Ini with no way to get out of it. Only the C19s are affected. The problem existed with the early version of this size Altivar 58 drive in the summer of 2003. PowerSuite software version V1.5 does work normally with these units.

The current revision of keypad and firmware do not have this problem. Replace keypad VW3A58101U

CTA-ID : 2010459
Was this helpful?
What can we do to improve the information ?