Technical FAQs

Ask a Question

Why won`t the contacts close on 2510 Type M manual starter?

The device CANNOT be turned ON unless ALL three of the thermal units are properly installed AND the unit is RESET. Getting the unit to reset requires a substantial amount of force when pressing the STOP/RESET button.



CTA-ID : 2009984
Was this helpful?
What can we do to improve the information ?