Technical FAQs

Ask a Question

What is parameter COd used for on the ATV28 ?

Issue:  What is parameter COd used for on the ATV28 ?
 
Product Line:  ATV28
 
Environment:  All
 
Cause:  password
 
Resolution:  This code is used if you want to enter a password so you can limit the access to the drive parameters.

This parameter can only be seen and accessed using a remote display module or PC software.

Access code: 0 to 9999. Value 0 (factory setting) does not prevent access.  All other values lock access to the SEt-, drC- and I-O menus.

To lock access to the drive controller, the code can be incremented using up and down arrow keys then saved using  (ENT) key.

To aaccess the menus on a drive controller which is locked by a code, the code cand be incremented using up and down arrow keys and confirmed with (ENT) key.



 
Was this helpful?
What can we do to improve the information ?