Technical FAQs

Ask a Question

Why is ATV58HC19N4XZU version 5.2 IE09 unit getting Ini fault?

This is a communication issue between keypad and the control basket for that size unit. This was only a problem when the ATV58HC19N4 drive was first introduced to the US market in 2003. A new keypad should resolve the issue.
The correct keypad part number is VW3A58101U.

CTA-ID : 2010445
Was this helpful?
What can we do to improve the information ?