Technical FAQs

Ask a Question

What is the energy savings for an ATS48 softstart?

The energy savings on a softstart for the most part is minimum.  The Altistart Soft Start does not offer an energy-saver feature.

If available, energy saver features on soft starters are intended to improve the motor efficiency.

Observe bulletin 8638PD9604R12/97 for more information on this.

CTA-ID : 2010439
Was this helpful?
What can we do to improve the information ?